Add a GAA Unit Capacity Record

Steps

  1. Access the GAA Unit for which you want to add a GAA Unit Capacity record.
  2. Select the Capacity tab.

    A list of GAA Unit Capacity records defined for the selected GAA Unit appears.

    Unit Capcity Record

    Note: When you add a GAA Unit record, a GAA Unit Capacity record is automatically created with the values defined in the capacity related fields in the GAA Unit record. As needed, you can modify the values in the available fields.

  3. In the upper-left corner of the Capacity section, select .

    The Add Capacity window appears.

    Add Unit Capcity Record

  4. As needed, enter the values in the available fields.

    Note: If you enter values in all the capacity-related fields and save the datasheet, the specified values will be used to perform various calculations in GAA. If you enter a value in Gross Maximum Capacity field only and save the datasheet, the values in other capacity-related fields will be populated as defined by NERC in the GADS DRI and those values will be used to perform various calculations in GAA.

  5. In the upper-right corner of the workspace, select Site:.

    Note: By default, the site to which the user is assigned appears.

  6. Select the site to which you want to assign the GAA Unit Capacity record.

    Note: If the GAA Unit Capacity record is assigned to the default site, it can be accessed only by users who have been assigned to the same site. The site selector component becomes read-only after it is saved.

  7. Select .

    Your changes are saved.

Copyright © 2018 General Electric Company. All rights reserved.