A job is used to extract information from the source and push it into GE Digital APM. Before you can initiate a job using the APM Connect Administration Center, you must first load the jobs into the APM Connect Administration Center. This is accomplished by importing the jobs from a .zip file. This topic describes how to import jobs into the APM Connect Administration Center.
Steps
In the Menu pane, in the Conductor section, select the Job Conductor tab.
On the Job Conductor toolbar, select Add.
The Execution task pane is activated.
In the Execution task pane, in the Label box, enter a label for the job.
In the Description box, enter a description for the Job.
This is a utility job that is optional and it does not load data. When the job is run, it clears temporary tables not removed from your IR database during the loading process. This can help reduce the amount of disk space used by the IR database.
create_dinoloader_db.zip
Creates Intermediate Repository database for DinoLoader.
Note: This job must be executed before you can initiate any data imports using the data loaders.
Restarts failed Equipment load from the point of failure.
IR_Equipment_TC_APM_load.zip
Restarts failed Technical Characteristics load from the point of failure.
IR_FLOC_APM_Load.zip
Restarts failed Functional Location load from the point of failure.
IR_FLOC_TC_APM_Load.zip
Restarts failed Technical Characteristics load from the point of failure.
IR_Task_APM_load.zip
Restarts failed Notification Management load from the point of failure.
IR_WorkHistory_To_APM_load.zip
Restarts failed Work History load from the point of failure.
Load_ID_List.zip
Allows large amounts of Asset IDs to be loaded into GE Digital APM.
SAP_Equipment.zip
Loads Equipment records to GE Digital APM.
SAP_Equipment_TechCharacters.zip
Loads Equipment Technical Characteristics records to GE Digital APM.
SAP_FunctionalLocation.zip
Loads Functional Location records to GE Digital APM.
SAP_FunctionalLocation_TechCharacters.zip
Loads Functional Location Technical Characteristics records to GE Digital APM.
SAP_Master_Interface.zip
Wrapper job for all SAP Adapters allowing easy configuration of multiple SAP jobs.
Note: This job can be used to run all of the Adapter jobs. It is recommended to use this job solely. Additionally, if you are using Multiple SAP systems you must use this job.
Allows for an email notification to be sent when a job or extraction fails. This report, the Failure Details report, provides the reason for why a record did not load.
EncryptString.zip
Used to encrypt passwords.
Extraction_Wrapper.zip
Wrapper job for all SAP Adapters allowing easy configuration of multiple SAP jobs.
Note: This job can be used to run all of the Adapter jobs. It is recommended to use this job solely. Additionally, if you are using multiple SAP systems you must use this job.
SAP_NotificationManagement.zip
Create SAP Notification from General Recommendations.