Deploy Maximo Adapters for the First Time

The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic GE Digital APM system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

Note: This GE Digital APM module is not available in the APM Now environment.

Important: If you are using SSL, make sure you have configured SSL correctly.

Step Task Notes
1 Deploy the APM Connect Base. This step is required.
2

In GE Digital APM, assign security users to one or more of the APM Connect Security Groups.

This step is required.
3 On the APM Connect sever, configure the context file. This step is required.
4 On the APM Connect server, encrypt passwords in the context file. None
5 On the APM Connect sever, import notification management file. This step is required.
6 In the APM Connect Administration Center, configure the context parameters. This step is required.
7 In the APM Connect Administration Center, create the intermediate repository database. None
8 Configure Site Reference Values. This step is required only if you want to modify the default configuration for Site References.
9

In Maximo, create object structures.

This step is required.
10 In Maximo, create web services. This step is required only if you are not using the REST web services.
11 In Maximo, configure the default password. This step is required.
12

In GE Digital APM, create EAM System records to identify your Maximo systems.

This step is required.

Related Information

Copyright © 2018 General Electric Company. All rights reserved.