Create EAM System Records

Steps

  1. Create a new record , using the EAM System family.

  2. In the Datasheet ID: box, select Maximo.

  3. In the Name box, enter the name of the Maximo system.

  4. If this system is the system to and from which you want to send data by default, select the Default EAM System? check box.

  5. In the System Type box, select Maximo.

  6. In the User ID box, enter a valid User ID.

  7. In the Password box, select .

  8. In the Enter EAM System Password window, in the Password box, enter the password that is associated with the specified user ID.

  9. In the Confirm Password box, reenter the password.

  10. Select OK.

  11. In the Web Service URL box, enter the URL for the Maximo Web Services that will extract the data.

  12. In the Language box, enter the code of the language for this connection (for example, EN).

  13. In the Service Request Family Name box, enter the table name for the Service Request in Maximo (this value is usually MISR).

  14. In the Work Order Family Name box, enter the table name for the Work Order in Maximo (this value is usually MIWO).

  15. In the WO or SR box, enter the default notification type to be created. This value can either be WO or SR.

  16. In the Default Site ID box, enter the Site under which the WO or SR should be created if it is not provided in the notification the system receives.

  17. Select .

    The EAM System record is saved.

  18. Select , and then select Test Connection.

    The connection parameters are verified, and the System ID box is populated with your EAM System ID.

Results

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.