Datablock Browser Dialog Box

The Datablock Browser Properties Viewer is where you can configure Datablock Browser properties.

Item IDs and Access Paths

Item IDs Browser

Displays the item IDs for every OPC server installed on the local computer. Use the plus and minus buttons to expand and collapse the list.

Access Paths Browser

Displays all available access paths for the selected item ID. Use the plus and minus buttons to expand and collapse the list.

NOTE: Not all OPC servers support access paths.

Item ID

Specifies the fully qualified item ID that you want to use. You can also complete the setting by browsing the OPC server. After you select an item ID and click OK, the Power Tool completes the item’s Item ID field.

Access Path

Specifies the access path that you want to use. You can also complete the setting by browsing the OPC server. After you select an access path and click OK, the Power Tool completes the item’s Access Path field.

If you do not want to include an access path, you can leave this field blank.

iFIX Process Database Tag

Enable iFIX PDB Tag Auto-creation

Enables the Tag Desc Prefix, iFix Database Tag Type, and Tag Name Prefix settings to allow you to automatically create database blocks in, and to add existing items to, the iFIX Process Database.

If you select this check box on the Database Tag dialog box it will also be selected on the Device Browser and Datablock Browser dialog boxes.

If you select this check box on the Device Browser dialog box it will also be selected on the Database Tag and Datablock Browser dialog boxes.

If you select this check box on the Datablock Browser dialog box it will also be selected on the Database Tag and Device Browser dialog boxes.

iFIX Database Tag Type

Specifies the type of datablock you are creating. This setting is available on the Database Tag, Device Browser, and Datablock Browser dialog boxes. This setting is available only if the Enable iFix PDB Tag Auto-creation check box is selected.

Valid Entries

  • AI – Analog Input
  • AO – Analog Output
  • DI – Digital Input
  • DO – Digital Output

Tag Desc Prefix

Specifies the description of the datablocks you are creating. This setting is available on the Database Tag, Device Browser, and Datablock Browser dialog boxes. This setting is available only if the Enable iFix PDB Tag Auto-creation check box is selected.

By default, "AG-" is displayed. "AG-" is an acronym for "Auto Generated" and indicates, in the iFIX Process Database, that the tag has been automatically generated. Adding AG- to the description provides you with a way to search the iFIX Process Database for the tags you created in the OPC Client Power Tool.

Valid Entries

Up to 40 characters.

Tag Name Prefix

Specifies the prefix of the datablocks that you are creating. This setting is available on the Database Tag, Device Browser, and Datablock Browser dialog boxes. This setting is available only if the Enable iFix PDB Tag Auto-creation check box is selected.

NOTES:

  • You cannot duplicate tag names in the iFIX process database. When adding the same item with a different tag type to the iFIX process database, you must add a Tag Name Prefix to the item name.
  • Tag names must contain only alphanumeric characters. A tag name containing non-alphanumeric characters (e.g., *, ~) will prevent the tag from being added to the iFIX process database.

See Also