Setting Up the Auto Alarm Manager Timers
To set up the
Auto Alarm Manager timers:
- On the Sender node, in Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.
-Or-
In Ribbon view, on the Applications tab, in the System & Security group, click SCU.
- On the Configure menu, click Auto Alarm Manager.
- Select the Enable option.
- Select the Advanced button.
- In the Send Timeout field, enter the number of seconds that the Sending node has to report alarms to the Receiving node.
- In the Receive Timeout field, enter the number of seconds that the Sending node waits for an acknowledgement from the Receiving node that the alarms were delivered successfully.
- Click OK.