NETDIAG provides comprehensive network diagnostic information and stores its information in the file NETDIAG.DAT. This file resides in the Application path.
To run NETDIAG, click the Start button, click Run, and then type the following on the command line:
NETDIAG<Enter>
The following command line parameters are available for NETDIAG:
- -D - Creates Netdiag.dat under the [iFIX install folder]\APP folder.
- -DT - Creates NetdiagFIX[MMDDYYHHMMSS].dat under the [iFIX install folder]\APP folder. For example: "netdiagFIX042821132712.dat"