Using PING

PING is a TCP/IP diagnostic utility that helps to isolate network hardware problems and incompatible configurations by allowing you to verify a physical connection to a remote computer. PING must run successfully before iFIX can run properly. To run PING, type the following from the command line:

PING SCU_nodename<Enter>

For example, to test a connection from a View node to the local SCADA node, SCADA01, type the following:

PING SCADA01<Enter>

See your TCP/IP manuals for additional information on using PING.

 

See Also