Viewing Auto Alarm Manager Statistics
Using the AAM tabbed page in Mission Control, you can view run-time messages and troubleshooting statistics in a scrollable window.
The lower portion of the tabbed page contains fields that the Auto Alarm Manager uses to display alarm statistics. As alarms are received from the user queue, the number of the alarms is displayed, and errors relating to the alarms are displayed in the remaining fields from top to bottom. These statistics can help you troubleshoot the sending and receiving of alarms. To reset the displayed values, click Reset Statistics.
For a description of the fields on the AAM tabbed page, refer to the Auto Alarm Manager Tabbed Page Fields section.
Refer to the Troubleshooting the Auto Alarm Manager section Implementing Alarming and Messages electronic book for an explanation of the messages that are displayed in the Auto Alarm Manager.