Even if you have configured an I/O driver to automatically start, you may still want to manually start or stop the I/O driver. For example, when troubleshooting, you may need to stop the driver temporarily and then restart it.
To start I/O drivers manually in Mission Control, click the I/O Control tab. You can select a driver name from the Drivers list box. To start the selected driver, click Start. To stop the driver, click Stop.
For a description of the fields on the I/O Control tabbed page, refer to the I/O Control Tabbed Page Fields section.