Text Recipe Format

Using the Save As command, you can save master and control recipes as master text and control text recipes. The difference between these file formats is that master and control recipes are binary files. Master text and control text recipes are text files that can be edited with a text editor. To use the Save As command, refer to the section Using the Save As Command.

File Format

Master text and control text recipes share the same format and have the following general format:

The following sections describe each portion of the recipe.

See Also