The Save As command allows you to save the current recipe under a new name. The Save As command also allows you to save the recipe in one of the following recipe types:
- Master recipe
- Control recipe
- Master text recipe
- Control text recipe
If you do not change the name or recipe type, the Save As command makes a backup copy of the original and overwrites the original recipe.
;However, when you change the recipe's name or type, the Save As command does not overwrite the original recipe — it creates a new one. This feature lets you create control recipes from master recipes and master recipes from control recipes. It also lets you create multiple versions of a master or control recipe by repeatedly saving it with different names.
The Save As command is also useful when saving a new recipe. When saving this type of recipe, the command allows you to create a recipe by specifying a name and a recipe type.
When you select Save As, the Recipe Mod Log dialog box appears, if the audit trail is enabled. For more information about this dialog box, refer to the section Saving a Recipe.
After you enter the text you want in the Mod Log field, select the Save As button. The standard Save As dialog box appears. To save the recipe, type its name in the File Name field and click OK.