Recipe Header
Following the recipe header template is the recipe header section. This section begins with the following line:
[header]
Information from the Recipe header fields and certain dialog boxes immediately follows this line. These fields appear in the same order as the recipe header template shown above. Each field is on its own line and ends with a comma. If the field is blank, the line in the recipe contains only the comma.
Example: Reader Header
MASTER,
FERMENTER1,
BEER,
100,
BLS,
NONE,
,
FERMENT1:ILK1.F_CV
,
Summary Audit Trail,
Beer1.TGE,
50
If you edit a text recipe, you can omit any information you want but the commas must be included, as shown in the above example.