To create a custom
lookup table:
- In the iFIX WorkSpace system tree, double-click the Globals folder.
- Right-click the User icon and select Create Threshold Table from the pop-up menu. The Custom Lookup Table dialog box appears.
- In the Source Property Type list, select the input data type.
- In the Objects Property Type list, select the output data type.
- Select either the Range Comparison option (to define a range of values for each row in the lookup table) or the Exact Match option (to define a single digital value for each row in the lookup table).
- Make sure you have the correct number of rows in the table. If you do not, click the Insert Row button to add a row. If you have too many rows, click the Delete Row button to remove a row from the table. To modify a row, click the Modify button to open the New Level dialog box to make your changes.
- Do one of the following:
- Enter the high and low values for each row in the lookup table.
- Enter a single lookup value in the Value column for each row in the lookup table.
- Enter or select the comparison value for each row in the lookup table by doing one of the following:
- If you want to define a color, double-click the color you want to modify and select a new one from the Color dialog box when it appears.
- If you want to enter a string or a numeric value, enter it into the cell.
- If you want the object to blink, enter a blink value for each row in the lookup table.
- If you want to enter global toggle values, shared lookup objects, or other options such as the toggle rate, click the Advanced button. The Advanced Lookup Options dialog box appears.
- In the Advanced Lookup Options dialog box, enter the required settings and click OK.
- Click OK.
See Also