Advanced Lookup Options Dialog Box
The Advanced Lookup Options dialog box displays the following items:
Toggle Source
Allows you to enter a data source or expression to provide an additional animation to an object.
Toggle Value
Allows you to specify a second output color to which you want to convert the input value or range of values in the lookup table, based on the value of the data source in the Toggle Source field.
Table
Allows you to override the default lookup table completely and use a user-defined lookup table that is defined in the User Global page.
Toggle Rate
Allows you to modify the blink rate of the animations that are tied to the selected object, if you have specified a second data source through the Toggle Source field.
Unmatched Level
Allows you to specify the color value for the data if the conversion does not match a level that is defined in the lookup table.
Tolerance for Exact Match Table
Allows you to specify the allowable deviation from the exact match table. For example, if the exact match table has a configured level of 20, and you enter a tolerance of .1, then the conversion will proceed even with a value of 19.9.