Custom Lookup Table Dialog Box
The Custom Lookup Table dialog box displays the following items:
Source Property Type
Allows you to specify the input data type for which you want to configure a custom lookup table. You can create a custom lookup table for the following data types: Boolean, integer, float, and string values.
Object Property Type
Allows you to specify the output data type that corresponds to the input data type specified in the Source Property Type field. You can specify the following data types as output values: Boolean, integer, float, string, and color.
Exact Match
Allows you to specify that incoming data must exactly match the configured input value in the lookup table in order to format the data as the corresponding output value.
Range Comparison
Allows you to specify that incoming data must fall within a range of input values in the lookup table in order to format the data as the corresponding output value.
Grid
Allows you to configure the lookup table for this property. Double-click any cell in the table to configure the input data, output data, and toggle (blink to) data.
Insert Row
Inserts a new row into the data conversion table.
Modify Row
Displays the New Level Dialog Box so that you can modify an existing row in the data conversion table.
Delete Row
Deletes an existing row of the data conversion table.
Advanced
Displays the Advanced Lookup Options Dialog Box that allows you to configure several more lookup options.