Understanding Signal Conditioning

Very often raw values from your process hardware are not meaningful to operators. This is particularly true when the hardware reports values in a numeric format, such as an unsigned integer, to indicate how full a tank is. In this situation, what is needed is a way to map the range of values you receive into a different range of values. Many I/O drivers provide this ability by applying signal conditioning.

Signal conditioning converts the data received from the process hardware into a format that is easily recognizable by operators. You can apply signal conditioning by selecting the type you want to use from a block's Signal Conditioning field.

Example: Understanding Signal Conditioning

Suppose you have a 700-gallon water tank and you want to display how much water is in the tank. You can display the tank's water level as:

  • Unscaled integer received from your process hardware
  • Gallons
  • Percent filled

For this example, assume the I/O driver sends an unsigned integer to the process database (that is, 0 to 65535). The following table lists sample high and low EGU limits you could assign to the input block. These settings scale the incoming values to display the tank's water level in percent filled and in gallons.

Example Block EGU Limits 

Operator Display:

Limit Settings:

Unsigned Integer

0 to 65535

Percent

0 to 100

Gallons

0 to 700

The following figure shows the values that are displayed when the tank is full, half full, and empty.

Scaling Values

 

See Also