Supported Configurations for AAM

The supported configurations for the Auto Alarm Manager (AAM) with TCP/IP are depicted in the following figures.

Senders: FIX32 & iFIX, Receiver: iFIX

If the Senders are a mix of FIX32 and iFIX, the Receiver must be iFIX:

Senders: FIX32, Receiver: FIX32 or iFIX

If all Senders are FIX32, then the Receiver can be either iFIX or FIX32:

Senders: iFIX, Receiver: iFIX

If all Senders are iFIX, then the Receiver must be iFIX:

IMPORTANT:

  • You cannot use an iFIX Sender and FIX32 Receiver. This scenario is unsupported.
  • Nodes that you switch to TCP/IP networking can no longer communicate to nodes using NetBIOS. You cannot run AAM with NetBIOS and TCP/IP configured on the same computer.
  • Supported configurations are Point-to-Point (node-to-node) and Point-to-LAN configurations.

 

See Also