Point-to-Point Configuration

You can set up nodes in a Point-to-Point configuration so that they communicate over LAN adapter x by opening the Network control panel on the Sending and Receiving nodes, and then configuring the specified LAN adapters shown in the following figure.

Point-to-Point Configuration

NOTE: You can use this configuration to dial into the Sending node from the Receiving node. iFIX or FIX is installed on both the RAS Client and RAS Server in this configuration. For more information on valid iFIX and FIX configurations, refer to the "Supported Configurations" section of this document.