Tag Functions
Tag Functions Overview
Tag functions provide browse, add, modify, and delete access to the configured tags on a server. You can retrieve the properties for each tag with User API calls. For example, you can retrieve user-defined collection parameters for a tag before collection, or retrieve user-configured display parameters to prepare for plotting.
You can retrieve string and numeric tag properties. Every tag property is classified as string or numeric (double float). For example, Boolean properties are converted to double float and time data type properties are converted to string.
You can add, delete, or modify tags using the User API.
You can browse tags in three different ways. The simplest mode uses ihuFetchTagCache
to filter by tagname. To filter by additional properties, such as data type or collector name, use ihuFetchTagCacheEx
. Finally, to browse in multiple browser windows at the same time, for example, to compare the tags on one server with those on another server, use ihuFetchTagCacheEx2
or ihuFetchTagCacheEx3
.
Tag Functions
- ihuCreateTagCacheContext
- ihuFetchTagCache
- ihuFetchTagCacheEx
- ihuFetchTagCacheEx2
- ihuFetchTagCacheEx3
- ihuGetTagNameCacheIndex
- ihuGetTagNameCacheIndexEx2
- ihuGetNumericTagPropertyByTagname
- ihuGetNumericTagPropertyByIndex
- ihuGetNumericTagPropertyByIndexEx2
- ihuGetStringTagPropertyByTagname
- ihuGetStringTagPropertyByTagnameEx2
- ihuGetStringTagPropertyByIndex
- ihuGetStringTagPropertyByIndexEx2
- ihuTagAdd
- ihuTagDelete
- ihuTagRename
- ihuTagCacheCriteriaClear
- ihuTagCacheCriteriaClearEx2
- ihuTagCacheCriteriaSetStringProperty
- ihuTagCacheCriteriaSetStringPropertyEx2
- ihuTagCacheCriteriaSetNumericProperty
- ihuTagCacheCriteriaSetNumericPropertyEx2
- ihuTagClearProperties
- ihuTagSetStringProperty
- ihuTagSetNumericProperty
- ihuCloseTagCache
- ihuCloseTagCacheEx2
Tag Property Value Types
The following table lists the current set of tag properties that are exposed, and indicates whether they are numeric or string. Use ihuGetNumericTagPropertyByIndex and ihuGetNumericTagPropertyByTagname to retrieve numeric properties, and ihuGetStringTagPropertyByIndex and ihuGetStringTagPropertyByTagname to retrieve string properties.
Property | Value Type |
---|---|
ihuTagPropTagname | String |
ihuTagPropDescription | String |
ihuTagPropEngineeringUnits | String |
ihuTagPropComment | String |
ihuTagPropDataType | Numeric |
ihuTagPropFixedStringLength | Numeric |
ihuTagPropInterfaceName | String |
ihuTagPropSourceAddress | String |
ihuTagPropCollectionType | Numeric |
ihuTagPropCollectionInterval | Numeric |
ihuTagPropCollectionOffset | Numeric |
ihuTagPropLoadBalancing | Numeric |
ihuTagProptime stampType | Numeric |
ihuTagPropHighEngineeringUnits | Numeric |
ihuTagPropLowEngineeringUnits | Numeric |
ihuTagPropInputScaling | Numeric |
ihuTagPropHighScale | Numeric |
ihuTagPropLowScale | Numeric |
ihuTagPropCollectorCompression | Numeric |
ihuTagPropCollectorDeadbandPercentRange | Numeric |
ihuTagPropArchiveCompression | Numeric |
ihuTagPropArchiveDeadbandPercentRange | Numeric |
ihuTagPropSpare1 | String |
ihuTagPropSpare2 | String |
ihuTagPropSpare3 | String |
ihuTagPropSpare4 | String |
ihuTagPropSpare5 | String |
ihuTagPropReadSecurityGroup | String |
ihuTagPropWriteSecurityGroup | String |
ihuTagPropAdministratorSecurityGroup | String |
ihuTagPropLastModified (not currently implemented) | String |
ihuTagPropLastModifiedUser | String |
ihuTagPropInterfaceType | Numeric |
ihuTagPropStoreMilliseconds | Numeric |
ihuTagPropUTCBias | Numeric |
ihuTagPropNumberOfCalculationDependencies | Numeric |
ihuTagPropCalculationDependencies (only the first dependency is returned) | String |
ihuTagPropAverageCollectionTime | Numeric |
ihuTagPropCollectionDisabled | Numeric |
ihuTagPropArchiveCompressionTimeout | Numeric |
ihuTagPropCollectorCompressionTimeout | Numeric |
ihuTagPropDataDensity Note: Tag data density categories are minimum ( 1 ), medium (4 ), and maximum (7 ). | Numeric |
ihuTagPropNumberOfElements Note: If the NumberOfElements value is -1 , the tag is an array tag. | Numeric |
ihuCreateTagCacheContext
Use the ihuCreateTagCacheContext
function to create tag cache context to use in the ihuFetchTagCacheEx2
or ihuFetchTagCacheEx3
functions.
Prototype
void * IHUAPI ihuCreateTagCacheContext {
};
ihuFetchTagCache
Use this function to fetch a current set of tags and properties from the Historian server and place them into an API cache for subsequent queries, such as ihuGetNumericTagPropertyByTagname.
Prototype
ihuFetchTagCache {
in long serverhandle,
in MSO Char * tagmask,
out int * NumTagsFound
};
Remarks
The function retrieves properties for each tag received.
There is a single API tag cache. You must free the previous tag cache before you do another fetch from the same or a different server. Keep this in mind when you access the tag cache from multiple threads in the same application. Alternatively, use the ihuCreateTagCacheContext
and ihuFetchTagCacheEx2
or ihuFetchTagCacheEx3
functions.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuFetchTagCacheEx
Use the ihuFetcTagCacheEx
function to fetch a current set of tags and properties from the Historian server and place them into an API cache for subsequent queries, such as ihuGetNumericTagPropertyByTagname
.
Prototype
ihuFetchTagCacheEx {
in long serverhandle,
out int * NumTagsFound,
};
Remarks
This function uses the criteria set up by ihuTagCacheCriteriaSetStringProperty
and ihuTagCacheCriteriaSetNumericProperty
for tag browsing.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuFetchTagCacheEx2
Use the ihuFetchTagCacheEx2
function to fetch a current set of tags and properties from the Historian server and place them into an API cache for subsequent queries.
Prototype
ihuFetchTagCacheEx2 {
void * tagCacheContext,
long serverhandle,
MSO Char * tagmask,
int * NumTagsFound
};
Remarks
This function uses the criteria specified in ihuTagCacheCriteriaSetStringProperty
and ihuTagCacheCriteriaSetNumericProperty
for tag browsing.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuFetchTagCacheEx3
Use the ihuFetchTagCacheEx3
function to fetch a current set of tags and properties from the Historian server and place them into an API cache for subsequent queries.
Prototype
ihuFetchTagCacheEx3 {
void * tagCacheContext,
long serverhandle,
int * NumTagsFound
};
Remarks
This function uses the criteria specified in ihuTagCacheCriteriaSetStringProperty
and ihuTagCacheCriteriaSetNumericProperty
for tag browsing.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuGetTagNameCacheIndex
Use the ihuGetTagNameCacheIndex
function to find the index of the specified tagname in the cache. You can use the index for fast access in subsequent get property by index calls. This call only queries the API tag cache. It does not access the archiver.
Prototype
ihuGetTagnameCacheIndex {
in MSO Char *Tagname
out unsigned int *CacheIndex
};
Remarks
The value returned in CacheIndex
is a zero-based index suitable to be passed into the get property by index functions. The index is valid only if the function returns a success error code.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_TAGNAME
ihuGetTagNameCacheIndexEx2
Use the ihuGetTagNameCacheIndexEx2
function to find the index of the specified tagname in the cache. You can use the index for fast access in subsequent get property by index calls. This call only queries the API tag cache. It does not access the archiver.
Prototype
ihuGetTagnameCacheIndexEx2 {
Void *TagCacheContext,
MSO Char *Tagname
unsigned int *CacheIndex
};
Remarks
The value returned in CacheIndex
is a zero-based index suitable to be passed into the get property by index functions. The index is valid only if the function returns a success error code.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_TAGNAME
ihuGetNumericTagPropertyByTagname
Use the ihuGetNumericTagPropertyByTagname
function to retrieve the value of a specified numeric tag property from the API tag cache for a specified tag. This call queries the cache, but not the archiver. The tag property may have changed since the cache was fetched.
Prototype
ihuGetNumericTagPropertyByTagname {
in MSO Char *Tagname,
in ihuTagProperties TagProperty,
out double *Value
};
Remarks
The get by tagname function is slower than the get by index function because it loops through all tags in the cache to find the requested tag. To retrieve multiple properties for a tag, consider calling ihuGetTagnameCacheIndex
to get the cache index of a tag so that you can use the get by index functions.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_INVALID_TAGNAME
ihuGetNumericTagPropertyByIndex
Use the ihuGetNumericTagPropertyByIndex
function to retrieve the value of a specified numeric tag property from the API tag cache at a specified cache index. This call queries the cache, but not the archiver. The tag property may have changed since the cache was fetched.
Prototype
ihuGetNumericTagPropertyByIndex {
in int Index,
in ihuTagProperties TagProperty,
out double *Value
};
Remarks
Use the get property by index functions after you locate tags with ihuGetTagnameCacheIndex
, or when you want to iterate through all tags in the cache.
The index is zero-based.
Tags are returned from the cache in no particular order.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_INVALID_TAGNAME
ihuGetNumericTagPropertyByIndexEx2
Use the ihuGetNumericTagPropertyByIndexEX2
function to retrieve the value of a specified numeric tag property from the API tag cache at a specified cache index. This call queries the cache, but not the archiver. The tag property may have changed since the cache was fetched.
Prototype
ihuGetNumericTagPropertyByIndexEx2 {
void * TagCacheContext,
int Index,
ihuTagProperties TagProperty,
double *Value
};
Remarks
Use the get property by index functions when you do not know the tagname.
The index is zero-based.
Tags are returned from the cache in no particular order.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_INVALID_TAGNAME
ihuGetStringTagPropertyByTagName
Use the ihuGetStringTagPropertyByTagname
function to retrieve the value of a specified string tag property from the API tag cache for a specified tag. This call queries the cache, but not the archiver. The tag property may have changed since the cache was fetched.
Prototype
ihuGetStringTagPropertyByTagname {
in MSO Char *Tagname,
in ihuTagProperties TagProperty,
in int valuelength,
out MSO Char *Value
};
Remarks
The get by tagname function is slower than the get by index function because it loops through all tags in the cache to find the requested tag. To retrieve multiple properties for a tag, consider calling ihuGetTagnameCacheIndex
to get the cache index of a tag so that you can use the get by index functions.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_INVALID_TAGNAME
ihuGetStringTagPropertyByTagNameEx2
Use the ihuGetStringTagPropertyByTagnameEx2
function to retrieve the value of a specified string tag property from the API tag cache for a specified tag. This call queries the cache, but not the archiver. The tag property may have changed since the cache was fetched.
Prototype
ihuGetStringTagPropertyByTagnameEx2 {
void * TagCacheContext, MSO
Char * Tagname,
ihuTagProperties TagProperty,
MSO Char * Value,
int valuelength,
};
Remarks
The get by tagname function is slower than the get by index function because it loops through all tags in the cache to find the requested tag. To retrieve multiple properties for a tag, consider calling ihuGetTagnameCacheIndex
to get the cache index of a tag so that you can use the get by index functions.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_INVALID_TAGNAME
ihuGetStringTagPropertyByIndex
Use the ihuGetStringTagPropertyByIndex
function to retrieve the value of a specified string tag property from the API tag cache at a specified cache index. This call queries the cache, but not the archiver. The tag property may have changed since the cache was fetched.
Prototype
ihuGetStringTagPropertyByIndex {
in int Index,
in ihuTagProperties TagProperty,
out MSO Char *Value,
in int valuelength,
};
Remarks
Use the get property by index functions after you locate tags with ihuGetTagnameCacheIndex
, or when you want to iterate through all tags in the cache.
The index is zero-based.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_INVALID_TAGNAME
ihuGetStringTagPropertyByIndexEx2
Use the ihuGetStringTagPropertyByIndexEx2
function to retrieve the value of a specified string tag property from the API tag cache at a specified cache index. This call queries the cache, but not the archiver. The tag property may have changed since the cache was fetched.
Prototype
ihuGetStringTagPropertyByIndexEx2 {
void * TagCacheContext,
int Index,
ihuTagProperties TagProperty,
MSO Char * Value,
int valueLength,
};
Remarks
Use the get property by index functions when you do not know the tag name, or when you want to iterate through all tags in the cache.
The index is zero-based.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_INVALID_TAGNAME
ihuTagAdd
Use the ihuTagAdd
function to add or modify tags.
Prototype
ihuTagAdd {
in long serverhandle,
};
Remarks
This function uses serverhandle
as a parameter.
Tag names that contain question marks (?
) or asterisks (*
) are not added to the server.
Returns
ihuSTATUS_OK
: SuccessihuSTATUS_INVALID_PARAMETER
: Invalid input parametersihuSTATUS_LIC_TOO_MANY_TAGS
: Added tags exceed the licensed tag countihuSTATUS_ACCESS_DENIED
: You do not have rights to add tags
ihuTagDelete
Use the ihuTagDelete
function to delete tags from the server.
Prototype
ihuTagDelete {
in long serverhandle,
in MSO Char * tagname,
};
Remarks
This function uses serverhandle
and tagname
as parameters.
Returns
ihuSTATUS_OK
: SuccessihuSTATUS_INVALID_PARAMETER
: Invalid input parametersihuSTATUS_ACCESS_DENIED
: You do not have rights to delete tags
ihuTagDeleteEx
You can use the ihuTagDeleteEx
function to permanently delete a tag by passing TRUE
as a parameter.
Prototype
ihuTagDeleteEx {
in long serverhandle,
in MSO Char * tagname,
BOOL DeletePermanent
};
Remarks
Use DeletePermanent
to create a new tag with a previously used name. The ihuTagDeleteEx
function uses the following parameters:
serverhandle
: The Historian server from which to fetch tagstagname
: Name of the tag to be deleted, which must be returned in a tag browseDeletePermanent
: Permanently deletes a tag when set toTRUE
Returns
ihuSTATUS_OK
: SuccessihuSTATUS_INVALID_PARAMETER
: Invalid input parametersihuSTATUS_ACCESS_DENIED
: You do not have rights to delete tags
ihuTagRename
Use the ihuTagRename
function to rename tags.
Prototype
ihuTagRename {
in long serverhandle,
in MSO Char * OldTagName,
in MSO Char * NewTagName,
};
Remarks
This function uses the following parameters:
serverhandle
: The Historian 4.0 server from which to fetch tagsOldTagname
: Name of the tag to be renamedNewTagname
: New tag name
Returns
ihuSTATUS_OK
: SuccessihuSTATUS_INVALID_PARAMETER
: Invalid input parametersihuSTATUS_ACCESS_DENIED
: You do not have rights to rename tags
ihuTagRenameEx
You can use the ihuTagRenameEx
function to permanently rename a tag by passing TRUE
as a parameter.
Prototype
ihuTagRenameEx {
in long serverhandle,
in MSO Char * OldTagName,
in MSO Char * NewTagName,
BOOL TrueRename,
};
Remarks
You can permanently rename tags that you do not want to read and write with their previous names. This function uses the following parameters:
serverhandle
: The Historian 4.0 server from which to fetch tagsOldTagname
: Name of the tag to be renamedNewTagname
: New tag nameTrueRename
: Permanently renames a tag when set toTRUE
.
Returns
ihuSTATUS_OK
: SuccessihuSTATUS_INVALID_PARAMETER
: Invalid input parametersihuSTATUS_ACCESS_DENIED
: You do not have rights to rename tags
ihuTagCacheCriteriaClear
Use the ihuTagCacheCriteriaClear
function to clear any cached criteria before you set up tag browse criteria.
Prototype
void IHUAPI ihuTagCacheCriteriaClear();
};
ihuTagCacheCriteriaClearEx2
Use the ihuTagCacheCriteriaClear
function to clear any cached criteria before you set up tag browse criteria.
Prototype
void IHUAPI ihuTagCacheCriteriaClearEx2
(
void * TagCacheContext,
};
ihuTagCacheCriteriaSetStringProperty
Use the ihuTagCacheCriteriaSetStringProperty
function to set up tag browse criteria before you call ihuFetchTagCacheEx
.
Prototype
ihuTagCacheCriteriaSetStringProperty {
in ihuTagProperties TagProperty,
in MSO Char *Value,
};
Remarks
This function fetches a current set of tags and properties from the Historian server and places them into an API cache for subsequent queries, such as ihuGetNumericTagPropertyByTagname
.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_INVALID_TAGNAME
ihuTagCacheCriteriaSetStringPropertyEx2
Use the ihuTagCacheCriteriaSetStringPropertyEx2
function to set up tag browse criteria before you call ihuFetchTagCacheEx
.
Prototype
ihuTagCacheCriteriaSetStringPropertyEx2 {
void * TagCacheContext,
ihuTagProperties TagProperty,
MSO Char *Value,
};
Remarks
This function fetches a current set of tags and properties from the Historian server and places them into an API cache for subsequent queries, such as ihuGetNumericTagPropertyByTagname
.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_INVALID_TAGNAME
ihuTagCacheCriteriaSetNumericProperty
Use the ihuTagCacheCriteriaSetNumericProperty
function to set up tag browse criteria.
Prototype
ihuTagCacheCriteriaSetNumericProperty {
in ihuTagProperties TagProperty,
in double Value,
};
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_INVALID_TAGNAME
ihuTagCacheCriteriaSetNumericPropertyEx2
Use the ihuTagCacheCriteriaSetNumericPropertyEx2
function to set up tag browse criteria.
Prototype
ihuTagCacheCriteriaSetNumericPropertyEx2 {
void * TagCacheContext,
ihuTagProperties TagProperty,
double Value,
};
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_INVALID_TAGNAME
ihuTagClearProperties
Use the ihuTagClearProperties
function to clear tag properties before you add tags to a server.
Prototype
void IHUAPI ihuTagClearProperties()
};
ihuTagSetStringProperty
Use the ihuTagSetStringProperty
function to set string tag properties before you call ihuTagAdd
.
Prototype
ihuTagSetStringProperty {
in ihuTagProperties TagProperty,
in MSO Char *Value,
};
Returns
ihuSTATUS_OK
ihuTagSetNumericProperty
Use the ihuTagSetNumericProperty
function to set numeric tag properties before you call ihuTagAdd
.
Prototype
ihuTagSetNumericProperty {
in ihuTagProperties TagProperty,
in double.Value,
};
Returns
ihuSTATUS_OK
ihuCloseTagCache
Use the ihuCloseTagCache
function to free the API cache from memory. Be sure to close the tag cache when not in use to free memory and prevent accidental usage.
Prototype
ihuCloseTagCache {
};
Returns
ihuSTATUS_OK
in all cases
ihuCloseTagCacheEx2
Use the ihuCloseTagCacheEx2
function to free the API cache from memory. Be sure to close the tag cache when not in use to free memory and prevent accidental usage.
Prototype
ihuCloseTagCache {
void * TagCacheContext
};
Returns
ihuSTATUS_OK
in all cases