Archiver Functions
Archiver Functions Overview
This group of functions provides a means to read and write a set of archiver properties. A minimum of properties (only those related to reads, writes, and tag browses) are available. See the code comments in the Historian User API header (ihuapi.h) for more details.
Archiver Functions
ihuSetArchiverProperty
Use the ihuSetArchiveProperty
function to change the value of specific Historian server options.
Prototype
ihuSetArchiverProperty
(long serverhandle,
MSO Char *ArchiveProperty,
MSO Char *PropertyValue)
The following properties are supported:
Property | Read/Write Access | Values | Description |
---|---|---|---|
ARCHIVER_PROP_CREATEOFFLINEARCHIVES | Read/Write | 1 , 0 | When set to 0 . (false) writes before the start time of the earliest archive are not enabled. Set to 1 only when you are migrating legacy data, and set the value back to 0 after migration is complete. Leaving this value set to 1 can cause excessive archive creation, especially when data is sent to the archiver out of order. |
ARCHIVER_PROP_CONFIGSERIALNUMBER | Read-Only | A large value that changes when the tag configuration changes. Typically used to cache configuration properties such as a set of tags. You can determine when your cache is out of date by comparing your saved serial number with the current serial number. | |
ARCHIVER_PROP_ACTIVEHOURS | Read/Write | 1-232800 hours (30 years) | The number of hours before the present time that the archive data became read-only. When migrating legacy data, you might need to set a large value. |
SECURITY_PROP_STRICTCLIENTAUTHENTICATION | Read/Write | 1 . 0 | Enables or disables strict client authentication. Set to 1 (true) by default for new Historian installations. When set to 1 , only version 4.7 or later clients can access the Historian server. |
SECURITY_PROP_STRICTCOLLECTORAUTHENTICATION | Read/Write | 1 . 0 | Enables or disables strict collector authentication. Set to 1 (true) by default for new Historian installations. When set to 1 , only version 4.7 or later collectors can access the Historian server. |
Returns
The ihuSetArchiverProperty
returns the following values:
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_OK
ihuSTATUS_ACCESS_DENIED
To change this property... | You must be a member of this group... |
---|---|
ARCHIVER_PROP_CREATEOFFLINEARCHIVES | ihArchive Admins or ihSecurity Admins |
ARCHIVER_PROP_ACTIVEHOURS | ihArchive Admins |
SECURITY_PROP_STRICTCLIENTAUTHENTICATION | ihArchive Admins |
SECURITY_PROP_STRICTCOLLECTORAUTHENTICATION | ihArchive Admins |
ihuGetArchiverProperty
Use the ihuGetArchiverProperty
function to read the value of certain archiver properties.
Prototype
ihuGetArchiverProperty {
in long serverhandle,
in MSO Char *ArchiveProperty,
out MSO Char *PropertyValue
};
Remarks
To read properties, you must be a member of the ih Readers security group. There is no need for you to be a member of the ih Security Admins or ih Archive Admins groups, unless you want to change property values.
Returns
ihuSTATUS_OK
ihuSTATUS_INVALID_PARAMETER
ihuSTATUS_ACCESS_DENIED