OSI PI Distributor Configuration
Configuring an OSI PI Distributor
About this task
Procedure
Tag Attributes Available in Browse
Historian Tag Browse Attribute | OSI PI Tag Attribute |
---|---|
Browse Source Address | Tag |
Description Property | Descriptor |
Engineering Unit Description | Engunits |
Hi Engineering Units | Zero+span |
Lo Engineering Units | Zero |
When entering tags manually, it is important to match the Historian tag data type with the data type of the OSI PI tag. See OSI PI Collector and Distributor Supported Data Types.
Regardless of how you add tags to Historian, you should match the timestamp resolution. If your OSI PI tag is using timestamps with milliseconds, then configure your Historian tag to store timestamps with millisecond resolution as well.
The OSI PI distributor reads data from the Historian tag displayed in the Tag Source Address field, and sends it to the OSI PI tag name displayed in the Spare 1 field. To control the source and destination tags, change the Tag Source Address and Spare 1 fields.
OSI PI Collector and Distributor Supported Data Types
OSI PI Tag Types | Recommended Historian Data Type |
---|---|
INT32 | Single Integer, Double Integer |
FLOAT16, FLOAT32 | Float |
FLOAT64 | Double Float |
PISTRING | Variable String |
DIGITAL | Single Integer The accompanying digital states are transferred from OSI PI into Historian upon initialization of the collector. |
Data Quality Mapping
Data quality mapping from Historian to OSI PI Data Archive is restricted to good
/bad
. OSI PI's subtypes are not currently mapped by Historian.
Starting and Stopping the OSI PI Distributor Service
About this task
To start/stop the OSI PI Distributor service