Migrating Advanced Historian Data
Migrating Advance Historian Data
About this task
Before you begin
Procedure
Advanced Historian to Historian Migration Utility
- Advanced Historian Connection Information Displays information for the Advanced Historian machine you are migrating your historical data from.
- Historian Information Displays the information for the Historian Server that you want to migrate your historical data to.
- Migration Options Allows you to select all or specific tag masks and set the time range for migration.
- Migration Status Displays the current status of the migration.
- Migration History Displays the history of all migrations that have occurred on that machine.
Advance Historian Connection Information
The Advanced Historian Connection Information section displays information for the Advanced Historian machine you are migrating your historical files from.
Field | Description |
---|---|
Computer Name | The name of the machine you want to migrate the Advanced Historian data from. |
Username and Password | The username and password, if you had Advanced Historian security configured for archives. |
Historian Information
The Historian Information section displays the information for the Historian Server that you want to migrate your historical data to.
Field | Description |
---|---|
Computer Name | The Historian Server to migrate Advanced Historian tags and data to. |
Username and Password | If you have created and established Security Groups in your Historian Security Environment, you may need to enter the username and password here. By default, if you do not supply any information, the current logged in user will be checked. For more information on setting up Historian Security, refer to Implementing Historian Security. |
Migration Option
The Migration Options section allows you to select all or specific tagmasks and set the time range for migration
Field | Description |
---|---|
Tagname Mask | Specify certain tags for migration only (NODE1:* for instance) or select all tags (*). |
Starting Date | Select a starting date for migrating data. |
Ending Date | Set an ending date for migrating data. Note: The Migration Utility migrates data up to but not including the specified Ending Date. Carefully select your Ending Date to ensure that you include all required data in the migration. |
Configure New Tags As Required | Specify whether the Migration Utility automatically creates tags upon migration, or migrates data only for tags that already exist in the Historian tag database. This allows you to manually create the tags you want to migrate in Historian first, then run the migration only for those tags. |
Use Tag Configuration from iFIX | Maintains tag specific configuration for iFIX tags. If you do not select this option, Historian uses its tag configuration default settings when migrating iFIX tags. For example, if you have an EGU set to 25-55 in an iFIX tag and you clear this option, the tag migrates with an EGU of 0-100. |
Allow Updates to Existing Data | Allows Historian to replace data if data already exists for the tag at that timestamp. |
End of Collection Marker | Write a bad data quality data point for each tag when the migration concludes. Select this option if you do not want your trend applications to display a continuous plot of the last good sample for that Historian tag. |
Migration Status
Displays the current status of the migration progress. The Migration Status window provides real time migration status including the currently migrating tag and the tag range (2 of 1000) status. Migration Status window also allows you to start the migration process and abort it once it has started.
Migration History
Displays a log of what times and tag masks were migrated and the status (success/failure) of that migration. The information displayed in the Migration History window is also available in the log file, typically located in the C:\Historian Data\LogFiles folder.
Migrating Your Groups
About this task
Procedure
Migrating Existing Advance Historian Data
About this task
To migrate Advanced Historian data from an existing Advanced Historian node to your Historian Server:
Procedure
Migrating Remote Advanced Historian Data
About this task
Before you begin
If this procedure is not run as listed, you may experience problems inserting a chart control into the iFIX WorkSpace, running any programs using fixtools.dll or fixhdadll.dll, or running certain Historian features. Several *.dll(s) are replaced by older versions by the Advanced Historian . When Advanced Historian is removed, it replaces the older versions with the originals and Historian works correctly.
Procedure
Recommended Software Installation Order
- Install iFIX 4.5 or higher.
- Reboot your computer.
- Install Advanced Historian
- Select Custom Installation with ONLY Client install.
- Reboot your computer.
- Install Historian completely.