Workflow for Using the Server-to-Server Distributor
To use the Server-to-Server distributor, you must perform the following tasks:
Number | Task | Notes |
---|---|---|
1 | Install the collectors on the source Historian server. | This step is required. This will place the collector binaries on the machines. |
2 | Add an instance of the Server-to-Server distributor on the source Historian server. | This step is required. |
3 | Start the Server-to-Server distributor | This step is required. |
4 | Configure the Server-to-Server distributor. | This step is required only if you want to change the default values. |
5 | Create a destination tag. You can do so by browsing for the tag, adding it manually, or copying a tag. | This step is required. The naming convention of the tag is
If
configured, the tag will contain a prefix. |