Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.
Configuring Deep Data Tree Warnings
About this task
Reading and writing to deep trees with large time ranges can be very inefficient. Create a MaxIndexRecursionDepth registry key to configure the depth at which the archiver will warn about deep data trees.
Procedure
From the Start menu, select Run, and then enter Regedit.
Open the following key folder: HKEY_LOCAL_MACHINE\SOFTWARE\Intellution, Inc.\iHistorian\Services\DataArchiver
Create a value as DWORD called MaxIndexRecursionDepth.
Set MaxIndexRecursionDepth to a number higher or lower than the default value of 900.
To get more warning messages, set a smaller number if you have an archive which is 10 to 100 deep.
Select OK.
Close the Registry Editor.
Restart the archiver for the changes to take effect.