Set a Default Data Store

About this task

When you set a default data store, if you do not specify a data store while adding a tag, it is added to the default data store.

Procedure

  1. Access the system in which you want to set the default data store.
  2. Select Locations.
    The current default data store appears below DEFAULT DATA STORE.
  3. Next to DEFAULT DATA STORE, select .
    The DEFAULT DATA STORE window appears, displaying a list of data stores in the system.
  4. Select the data store that you want to set as default, and then select Set as Default.
    The data store is set as default.