The Configuration Section for the Simulation Collector

About this task

To access the Configuration section for the Simulation Collector:

Procedure

  1. Select a Simulation Collector from the list on the left and select the Configuration section.
  2. The Number of Tags field displays the number of tags currently added to the Simulation Collector. Edit the Number of Tags field to increase or decrease the number of Simulation tags available for addition to the Historian system.


  3. The Function Period field configures the period, in seconds, of the SIN,STEP, and RAMP functions implemented in the Simulation Collector.
    The default is 60 seconds.