Workflow for Using the Server-to-Server Collector
To use the Server-to-Server collector, you must perform the following tasks:
Number | Task | Notes |
---|---|---|
1 | Install the collectors on the machine on which you want to run the collector. | This step is required. This will place the collector binaries on the machine. |
2 | Install Remote Management Agents. | This step is required to manage collectors installed on a remote machine. |
3 | Add an instance of the Server-to-Server collector using Configuration Hub. | This step is required. |
4 | Configure the Server-to-Server collector using Historian Administrator. | This step is required only if you want to change the default values. |
5 | Create a destination tag. You can do so by browsing for the tag, adding it manually, or copying a tag. | This step is required. If configured, the tag will contain a prefix. |
6 | Assign a trigger to the tag that you have created, similar to assigning a trigger for the Calculation collector. | This step is optional. The trigger can be scheduled (polled) or unsolicited (event-based). When you use an event-based trigger, you must also set up a dependency list of one or more tags. For more information, refer to Create a Polled Trigger and Create an Unsolicited Trigger. |
7 | Create a formula similar to creating a formula for the Calculation collector. For instructions, refer to About Calculation Formulas. | This step is optional. You can expect thousands of tags per second to be processed, depending on your calculation formula. However, the destination server has a limited number of incoming events per second, which is shared by all the collectors. For instance, for a polled collection, you can expect to perform hundreds of calculations per second. Polled calculations, using calculated data functions, are slower than unsolicited calculations using the CurrentValue() function. |