Troubleshoot Historian Performance
There are many parameters that affect Historian Server performance and scalability. This topic emphasizes the parameters that help improve performance and scalability.
Buffer Memory Max
Buffer Memory Max allows you to specify the maximum memory buffer size that an archiver queue can take. Use this parameter to control memory allocation to the write queues. If you plan to collect large amounts of data with high update rates, increase the Buffer Memory Max size. Increasing the Buffer Memory Max size provides enough memory for write queues, thus increasing the Historian performance. Refer to The Global Options Section for more information.
Performance Counters
Historian provides a variety of performance counters that can be used to monitor how
well the application is performing. Using the following performance counters you can
determine the Historian Server performance and scalability:
- Perftag_GenericWriteQueueSize: displays the total number of messages present in the Generic Write queue.
- Perftag_FastReadQueueSize: displays the total number of messages present in the Fast Read queue.
- Perftag_CollectorDataWriteQueueSize: displays the total number of messages present in the Collector Data Write queue.
- Perftag_EventMonitorQueueSize: displays the total number of events present in the Event Monitor queue.
- Perftag_DataWriteQueueSize: displays the total number of messages present in the Data Write queue
- Perftag_ReadQueueSize: displays the total number of messages present in the Read queue
- Control archive transitions by having larger archive file size.
- Control update rate.
- Perform a backup when an archiver is in stable state.
- Control the caching evaluation period. Refer to Historian Performance Counters for more information.
System File Cache Tuning:
Historian allows you to specify the maximum disk cache memory that an archiver can
use. Ideally, Historian consumes 25% of system memory. If your computer has extra
memory, then you can increase the disk cache memory to optimize Historian
performance.
Note: You should not increase disk cache memory if you do not have
the necessary system resources.