Summary of Cygnet collector Features
The following table outlines the features of the Cygnet collector.
Feature | Capability |
---|---|
Browse Source for Tags | Yes (on CygNet Server that supports browsing) |
Browse Source for Tag Attributes | Yes |
Polled Collection | Yes |
Unsolicited Collection | Yes |
Timestamp Resolution | 100ms |
Floating Point Data | Yes |
Integer Data | Yes |
String Data | Yes |
Python Expression Tags | No |
Note: You must set Time Assigned by field to Source as Cygnet collector prefers to support unsolicited tags.