The Pause Data Collection API

Using the Pause Data Collection API, you can pause the data collection of a collector.
METHOD PUT
URI
https://<historianservername>/historian-rest-api/v1/collector/pausecollection/{interfaceName}
SAMPLE URI
https://<historianservername>/historian-rest-api/v1/collector/pausecollection/RSSERVER2012-02_Simulation
SAMPLE RESPONSE
{
    "ErrorCode": 0,
    "ErrorMessage": ""
}
SAMPLE cURL COMMAND
curl -i -H "Accept: application/json" -i -H "Content-Type: application/json" 
-H "Authorization: Bearer <TOKEN>” -X PUT https://<historianservername>/historian-rest-api/v1/collector/pausecollection/RSSERVER2012-02_Simulation

Response Parameters

Parameter Data Type Required? Description
ErrorCode Integer Yes For example, ErrorCode = 0 implies the operation was successful.
ErrorMessage String Yes For example, NULL.
Data String No Indicates if the task has been initiated.