Configuration of OPC Collector Specific Fields

Enter values for the OPC Collector-specific field parameters through the OPC Collector Maintenance Configuration section of Historian Administrator. The following table lists the descriptions of the collector-specific fields:

FieldDescription
OPC Server Prog IDOPC Prog ID of the locally installed OPC Server.
Read ModeRead Source (DEVICE or CACHE). See the OPC Specification on the OPC Foundation website.
First Browse CriteriA comma separated list of criteria used as Filter 1 in a browse for tags.
Second Browse CriteriaA comma separated list of criteria used as Filter 2 in a browse for tags.

Note that the Tag Filters in First Browse Criteria and Second Browse Criteria are used to filter the tags returned on a browse. You can add multiple strings to each filter, separated by commas. If a filter is supplied, a tag must have one of the identified strings in the tagname in order to be returned. Consider the tags within a filter to be OR'ed and Filters 1 and 2 to be AND'ed.

For example, USGB014 in Filter 1 and F_CV, B_CUALM in Filter 2 translates to: Give me all the tags that contain USGB014 AND contain F_CV OR B_CUALM.

Threading ModelMultithreaded or Apartment. Use apartment threaded for best compatibility. Use multithreaded for better performance if your server is also multithreaded
Configuration Changes

Certain OPC Servers cannot handle processing configuration changes online.

This field allows you to select whether your OPC Collector configuration changes are processed in real time or after shutting down and restarting the collector. Select the Made On-Line option to process any configuration changes immediately when you select the Update button. Select the Made After Collector Restart option to hold all configuration changes until you manually stop and restart the OPC Collector.

Starting and stopping the collector in the General section of the Collector Maintenance page does not constitute a manual restart. You must either start and stop the collector from the Services window or the Console window. For more information, refer to the Configuring the Data Collector for Automatic

Startup and the Running Collectors as Console Applications sections of the Historian Data Collectors manual.

Normally, changes are applied approximately 30 seconds after the last change.