HONORENDTIME
Normally, a query keeps searching through archives until the desired number of samples has been located, or until it gets to the first or last archive. However, there are cases where you would want to specify a time limit as well. For example, you may want to output the returned data for a RawByNumber query in a trend page, in which case there is no need to return data that would be off page.
In cases where you want to specify a time limit, you can do this by specifying an end time in your RawByNumber query and including the HONORENDTIME query modifier. Since RawByNumber has direction (backwards or forwards), the end time must be older than the start time for a backwards direction or newer than the start time for a forwards direction.
- Example using HONORENDTIME with RawByNumber Sampling Mode
-
Import this data to Historian:
[Tags] Tagname,DataType,HiEngineeringUnits,LoEngineeringUnits TAG1,SingleInteger,60,0 [Data] Tagname,TimeStamp,Value,DataQuality TAG1,09/18/2015 14:00:00.000,00,Good TAG1,09/18/2015 14:05:00.000,5,Good TAG1,09/18/2015 14:10:00.000,10,Good TAG1,09/18/2015 14:15:00.000,15,Good TAG1,09/18/2015 14:20:00.000,20,Good TAG1,09/18/2015 14:25:00.000,25,Good TAG1,09/18/2015 14:30:00.000,30,Good TAG1,09/18/2015 14:35:00.000,35,Good TAG1,09/18/2015 14:40:00.000,40,Good TAG1,09/18/2015 14:45:00.000,45,Good TAG1,09/18/2015 14:50:00.000,50,Good TAG1,09/18/2015 14:55:00.000,55,Good TAG1,09/18/2015 15:00:00.000,60,Good
- Without HONORENDTIME Query Modifier
-
set starttime='9/18/2015 14:00:00',endtime='9/18/2015 14:15:00' select Timestamp,Value,Quality from ihrawdata where tagname like TAG1 and samplingmode=rawbynumber and direction=forwardand numberofsamples=6
The output is as follows:
Time Stamp Value Quality 9/18/2015 14:00:00 0 Good NonSpecific 9/18/2015 14:05:00 5 Good NonSpecific 9/18/2015 14:10:00 10 Good NonSpecific 9/18/2015 14:15:0 15 Good NonSpecific 9/18/2015 14:20:00 20 Good NonSpecific 9/18/2015 14:25:00 25 Good NonSpecific In the above query, the endtime specified is ignored and 6 values are returned.
- With HONORENDTIME Query Modifier
-
set starttime='9/18/2015 14:00:00',endtime='9/18/2015 14:15:00' select TagName,Timestamp,Value,Quality from ihrawdata where tagname like TAG1 and samplingmode=rawbynumber and direction=forward and numberofsamples=6 and criteriastring=#honorendtime
The output is as follows:
Time Stamp Value Quality 9/18/2015 14:00:00 0 Good NonSpecific 9/18/2015 14:05:00 5 Good NonSpecific 9/18/2015 14:10:00 10 Good NonSpecific 9/18/2015 14:15:0 15 Good NonSpecific In the above query, the endtime specified is used and only 4 values are returned.
- Anticipated Usage
-
Use the HONORENDTIME modifier when you would want to specify a time limit to a query. For example, you may want to output the returned data for a RawByNumber query in a trend page, in which case there is no need to return data that would be offpage.