Configuration of File collector Specific Fields
Enter values for the File collector-specific field parameters through the File Collector Maintenance - Configuration section of Historian Administrator.
The collector-specific field descriptions are listed in the following table.
Field | Description |
---|---|
ScanInterval (seconds) |
Collector initiates import operation at beginning of the scan interval specified in this field.
Note: Changes to the Scan Interval do not take effect until the File collector is restarted. |
CSV File Specification | The file extension for a CSV file to be imported. |
XML File Specification | The file extension for an XML file to be imported. |
Purge Processed Files After(days) |
The contents of the Processed Files folder is automatically purged after the number of days specified in this field. |
Purge Error Files After (days) | The contents of the Error Files folder is automatically purged after the number of days specified in this field. |