Load Data into the Destination Historian Server

Before you begin

  1. Configure the ETL Load tool.
  2. Verify that the Historian ETL Load tool running on the destination Historian server is configured to watch the IIS Virtual folder for the incoming .zip files.

Procedure

  1. Run the Historian ETL Load Configuration file located in the Historian ETL Load folder.
    The Historian ETL Load Configuration window appears.
  2. Select Start Service.
    Tip: If the tool does not start as expected, access the logs using Windows Event Viewer.
    The data is loaded in the destination Historian server.