Data File Format
This topic provides the format of the content in a text file that contains tag data extracted by the Historian ETL Extract tool. Each line in the text file contains the following parameters, separated by commas:
Parameter | Description | Valid Values |
---|---|---|
Time | The time at which the data is captured. It is displayed in
the following format: <epoch format>:<nanoseconds,
human-readable> For example, if the value is
1601890328:76000000, then: The value after the colon is greater than 0 only if
the time resolution of the tag is milliseconds or
microseconds.
|
N/A |
Tag name | The name of the tag for which the data is captured. | Any tag that exists in the destination Historian server Note: If the AddTagAutomatically parameter is set to True, when you add a tag that does not exist in the Historian server, it will be created. |
Data value | The value of the data that is captured. | N/A |
Data type | The data type for the value that is captured. |
|
Quality | The quality of the data that is captured. |
|
Note:
- The BLOB data type is not supported.
- Comments are not captured.
- Data quality other than GOOD and BAD is not supported.