Changing Service Port Numbers

About this task

To change the port number of any of the Configuration Manager, Data Archiver or Diagnostics Manager:

Procedure

  1. From Historian Admin Console, change the Port Number from the Services page.
    Note: You cannot update the port number of a service which is already in use in the same machine.
  2. Ensure that the changed port numbers are updated in the registry which is located at HKEY_LOCAL_MACHINE\SOFTWARE\Intellution, Inc.\iHistorian\Services.
    If the port number is not updated, you must update it manually.
  3. Restart the corresponding service.
    For example, if you change the port number of the Data Archiver, then you must restart the Data Archiver service.