Adding a Domain User

Procedure

  1. Verify object type is Users or Groups.
  2. Verify the From This Location setting is your Windows domain:
    1. Click Locations to specify the domain, if required.
    2. Select Entire Directory or the specific domain underneath Entire Directory.
    3. Click OK.
  3. Click Advanced.
    The Advanced dialog box appears.
  4. Click Find Now.
  5. From the list of users, select the users or groups to add or enter the names of the users or groups you want to add in the bottom field.
  6. In the Advanced dialog box, click OK.
  7. In the Select Users dialog box, click OK.
  8. In the Group Properties dialog box, click OK.