Applying a Quick Time to a Trend Chart

About this task

Note: When you have two charts open and use the Quick Time Picker to change the time in the first chart and then attempt to use the Quick Time Picker to change the time in the second chart, the second chart does not reflect the duration you selected.

Procedure

  1. Create or select an active chart.
  2. To quickly select a time range, click one of the Quick Start times: 1h. 8h, 1d, 1w. and 1m.
    The new time range loads and displays in the X-axis of the chart.