Compatibility with Other GE Products
Several GE products work with Historian. The following is a general set of required versions to work with Historian.
Product | Supported Version |
---|---|
CIMPLICITY | 9.0, 10.0 |
iFIX | 5.9, 6.0, 6.1 |
Plant Apps | PA 7.2 SP5 SIM4, PA 8.0 |
Workflow | 2.5 SP4, 2.6 |
Operations Hub | 1.5, 1.6 |
* For customers using iFIX, there was a change in the HKEY_CURRENT_USER registry values for WebSpace and it will no longer work with the existing SIM. Ensure that you get the latest iFIX SIMs. The following article provides additional instructions: https://ge-ip.force.com/communities/en_US/Article/iFIX-Webspace-Strict-Historian-Authentication
** For Plant Apps customers using the ?Historian Type = ?GE Proficy Historian 3.0 ?
to connect to Historian 7.2, both the Enabled and Disabled options for Enforce Strict Client Authentication selection are supported.
** For Plant Apps customers using the ?Historian Type = ?GE Proficy Historian to connect to Proficy Historian 7.2, only the Disabled option for Enforce Strict Client Authentication selection is supported.
In Historian 5.0, the Historian HKEY_CURRENT_USER registry key values were changed. The programs accessing the server collection through the SDK are unaffected. Any program or script that directly accesses the registry keys or any Terminal Server login scripts that try to configure a list of servers by importing registry keys directly will no longer work. Such programs need to access the server collection via SDK calls, not directly.
Historian REST APIs are required to integrate between Historian and Operations Hub. Historian REST APIs are installed automatically when you install Historian web-based clients.