Simulate Demand Polling
This example simulates demand polling. In order for it to function, the following tags must be created.
Tag | Description |
---|---|
Polled Tag | A polled tag with a collection interval of the longest period you want between raw samples. Do not enable collector or archive compression. This tag should point to the same source address as the UnsolicitedTag . |
Unsolicited Tag | An unsolicited tag with a 0 or 1 second collection interval. This tag ensures you will be notified whenever changes occur. This tag should point to the same source address as the PolledTag . |
Combined Tag | An unsolicited calculation tag that is triggered by either the Polled Tag or Unsolicited Tag, and combines the raw samples of both into a single tag. Use a 0 or 1 second collection interval and use the following formula:
|