Detect Recovery Mode Inside a Formula
This example shows how to detect recovery mode or recalculation inside a formula. If there are individual tags, you do not want to perform a recovery.
Example Code
Dim MAXDIFF, TimeDiff
'Maximum difference in timestamps allowed (Must be > 2,
'units = seconds) MAXDIFF = 10
'Calculate time difference
TimeDiff = DateDiff("s", CurrentTime(), Now)
'Compare times, if difference is < MAXDIFF seconds perform calc
If TimeDiff < MAXDIFF Then
'Place calculation to be performed here:
Result = CurrentValue("DENALI.Simulation00001") Else
'Place what is to be done when no calc is performed here
Result = Null
End If