Historian ETL Workflow

To transfer data using Historian ETL, you must perform the following steps.
Step Number Description Notes
1 Extract data from Proficy Historian or PI Server. This step is required. It involves extracting tag data and compressing it so that it can be transferred to the destination Historian server.
2 Transfer the data using BITS, FTP, or any other file-sharing application. This step is required. It involves setting up the file-sharing application that you want to use and then transferring the data to the machine on which the destination Historian server is installed.
3 Load the data into the destination Historian server. This step is optional. It involves extracting the .zip files transferred by the file-sharing application and then loading the data into the destination Historian server.
Note: Depending on the use case, you can use these tools independently or together.