Archiver Backup/Restore Functions

You can use Archive Backup/Restore functions to backup archive data.

There are synchronous and asynchronous calls for loading archives, making a backup and removing an archive. The synchronous functions are typically used for smaller archives because the operation completes in a few seconds. The asynchronous functions are typically used for larger archives because the operation can takes longer, one minute or more, to complete.

Archive Backup/Restore functions are as follows:

ihArchiveBackup

This function is used to back up archive (.iha) files. If you are storing Alarms and Events in Historian, an IHA backup also backs up any alarms.

Prototype

ihArchiveBackup {
ihServerHandle hServer, // server handle returned from previous call to ihServerConnect 

ihArchiveDescriptor *ArchiveDescriptor,

ihString BackupFileName

);

Remarks

This function is used to back up the archive (.iha) files residing on the server specified. The ArchiveDescriptor specifies the archive name that you want to add and the DataStore name to which it should be added. The BackupFileName has the backup of the IHA file with the name and the file location that you specified. For example: C:\Program Files\Historian Data\Archives\myarchive.iha.

Returns

Returns StatusMessage
ihSTATUS_OK If the option was successfully read.
ihSTATUS_ACCESS_DENIEDIf you are not allowed to perform the operations. For most options you need to be a member of the ihArchiveAdmins group
ihSTATUS_API_TIMEOUTIf the option could not be read. You can try again later.
ihSTATUS_NOT_CONNECTED If you are not currently connected to the Data Archiver.
ihSTATUS_FAILEDFor any other type of error.

ihArchiveBackupEx

This function is used to back up the archive (.iha) files and process Windows messages at the same time.

Prototype

ihArchiveBackupEx {
ihServerHandle hServer,// server handle returned from previous call to ihServerConnect 

ihArchiveDescriptor *ArchiveDescriptor,

ihString BackupFileName, long hWnd);

Remarks

This function is used to back up the archive (.iha) files residing on the server specified. The ArchiveDescriptor specifies the archive name that you want to add and the DataStore name to which it should be added. The BackupFileName has the backup of the IHA file with the name and the file location that you specified. For example: C:\Program Files\Historian Data\Archives\myarchive.iha.

Returns

Returns StatusMessage
ihSTATUS_OK If the option was successfully read.
ihSTATUS_ACCESS_DENIEDIf you are not allowed to perform the operations. For most options you need to be a member of the ihArchiveAdmins group
ihSTATUS_API_TIMEOUTIf the option could not be read. You can try again later.
ihSTATUS_NOT_CONNECTED If you are not currently connected to the Data Archiver.
ihSTATUS_FAILEDFor any other type of error.

ihArchiveRegisterBackupCallBack

This function is used to register a callback which should be called after the ihArchiveBackup() function completes. Archive backup can take several minutes. By using this callback, your System API program can know that the backup is complete.

Prototype

ihArchiveRegisterBackupCallBack {
ihServerHandle hServer, // server handle returned from previous call to ihServerConnect 

ihArchiveBackupCallbackFunction CallbackFunction,
void *UserParameter
);

Remarks

The register callback will be performed when the Archive backup is completed on Historian.

Returns

Returns StatusMessage
ihSTATUS_OK If the option was successfully read.
ihSTATUS_ACCESS_DENIEDIf you are not allowed to perform the operations. For most options you need to be a member of the ihArchiveAdmins group
ihSTATUS_API_TIMEOUTIf the option could not be read. You can try again later.
ihSTATUS_NOT_CONNECTED If you are not currently connected to the Data Archiver.
ihSTATUS_FAILEDFor any other type of error.

ihArchiveRemove

This function is used to delete or unload an archive file. You can unload a file if you no longer need it at the current time but may need it later or in another archive. You can delete a file if you do not expect to need it again or if you have made a backup.

Prototype

ihArchiveRemove {
ihServerHandle hServer, // server handle returned from previous call to ihServerConnect 

ihArchiveDescriptor *ArchiveDescriptor,

ihBoolean ShouldDeleteFile

)

Remarks

This function is used to delete or unload the archive file residing on the server specified. The ArchiveDescriptor specifies the archive name that you want to add and the DataStore name to which it should be added. ShouldDeleteFile determines whether the file should be deleted or not.

The following are the scenarios which you can use with ihArchiveRemove() function:
If ShouldDeleteFile is:ZipRegistry enabledZip successfulThen...
TRUEYESYESArchive file is deleted.
TRUEYESNOThe archive file is not deleted but unloaded.
FALSEYESYESThe archive file is not deleted.
FALSEYESNOThe archive file is not deleted.
Returns
Returns StatusMessage
ihSTATUS_OK If the option was successfully read.
ihSTATUS_ACCESS_DENIEDIf you are not allowed to perform the operations. For most options you need to be a member of the ihArchiveAdmins group
ihSTATUS_API_TIMEOUTIf the option could not be read. You can try again later.
ihSTATUS_NOT_CONNECTED If you are not currently connected to the Data Archiver.
ihSTATUS_FAILEDFor any other type of error.

ihArchiveRemoveEx

This function is used to delete or unload the archive files and process Windows messages at the same time.

Prototype

ihArchiveRemoveEx {
ihServerHandle hServer, // server handle returned from previous call to ihServerConnect 

ihArchiveDescriptor *ArchiveDescriptor,

ihBoolean ShouldDeleteFile,

long hWnd
);

Remarks

This function is used to delete or unload the archive file residing on the server specified. The ArchiveDescriptor specifies the archive name that you want to add and the DataStore name to which it should be added. ShouldDeleteFile determines whether the file should be deleted or not.

The following are the scenarios which you can use with ihArchiveRemoveEX() function:

If ShouldDeleteFile is:ZipRegistry enabledZip successfulThen...
TRUEYESYESArchive file is deleted.
TRUEYESNOThe archive file is not deleted but unloaded.
FALSEYESYESThe archive file is not deleted.
FALSEYESNOThe archive file is not deleted.

Returns

Returns StatusMessage
ihSTATUS_OK If the option was successfully read.
ihSTATUS_ACCESS_DENIEDIf you are not allowed to perform the operations. For most options you need to be a member of the ihArchiveAdmins group
ihSTATUS_API_TIMEOUTIf the option could not be read. You can try again later.
ihSTATUS_NOT_CONNECTED If you are not currently connected to the Data Archiver.
ihSTATUS_FAILEDFor any other type of error.

ihArchiveRegisterRemoveCallback

This function allows you to register a callback for removing an archive. This callback function is called when you remove the archive from Proficy Historian.

Prototype

ihArchiveRegisterRemoveCallback {
ihServerHandle hServer, // server handle returned from previous call to ihServerConnect 

ihArchiveRemoveCallbackFunction CallbackFunction,

void *UserParamter
);

Remarks

To register a function as a callback, you must have a callback or a function with the same signature as ihArchiveRemoveCallback function, and then pass it to ihArchiveRegisterRemoveCallback.

Returns

Returns StatusMessage
ihSTATUS_OK If the option was successfully read.
ihSTATUS_ACCESS_DENIEDIf you are not allowed to perform the operations. For most options you need to be a member of the ihArchiveAdmins group
ihSTATUS_API_TIMEOUTIf the option could not be read. You can try again later.
ihSTATUS_NOT_CONNECTED If you are not currently connected to the Data Archiver.
ihSTATUS_FAILEDFor any other type of error.

ihArchiveAdd

This function is used to create a new archive or load an existing one.

Prototype

ihArchiveAdd {
ihServerHandle hServer, // server handle returned from previous call to ihServerConnect 

ihArchiveDescriptor *ArchiveDescriptor,

ihString FileLocation, ihBoolean ShouldCreateFile,

ihUNSIGNED long FileSize
);

Remarks

This function is used to create or load the archive file residing on the server specified. The ArchiveDescriptor specifies the archive name that you want to add and the DataStore name to which it should be added. Then, specify the FileLocation. To determine whether the file should be created or not with the specified FileSize, use ShouldCreateFile.

Returns

Returns StatusMessage
ihSTATUS_OK If the option was successfully read.
ihSTATUS_ACCESS_DENIEDIf you are not allowed to perform the operations. For most options you need to be a member of the ihArchiveAdmins group
ihSTATUS_API_TIMEOUTIf the option could not be read. You can try again later.
ihSTATUS_NOT_CONNECTED If you are not currently connected to the Data Archiver.
ihSTATUS_FAILEDFor any other type of error.

ihArchiveAddEx

This function is used to create a new archive or load an existing one.

Prototype

ihArchiveAddEx {
ihServerHandle hServer, // server handle returned from previous call to ihServerConnect 

ihArchiveDescriptor *ArchiveDescriptor,

ihString FileLocation, 

ihBoolean ShouldCreateFile, 

ihUNSIGNED long FileSize, 

long hWnd

);

Remarks

This function is used to create or load the archive file residing on the server specified. The ArchiveDescriptor specifies the archive name that you want to add and the DataStore name to which it should be added. Then, specify the FileLocation. To determine whether the file should be created or not with the specified FileSize, use ShouldCreateFile.

Returns

Returns StatusMessage
ihSTATUS_OK If the option was successfully read.
ihSTATUS_ACCESS_DENIEDIf you are not allowed to perform the operations. For most options you need to be a member of the ihArchiveAdmins group
ihSTATUS_API_TIMEOUTIf the option could not be read. You can try again later.
ihSTATUS_NOT_CONNECTED If you are not currently connected to the Data Archiver.
ihSTATUS_FAILEDFor any other type of error.

ihArchiveRegisterLoadCallback

This function allows you to register a callback for adding an archive file. That registered callback is called when you add the archive file in Historian. It can take several minutes to load large archive files, so by using callbacks your System API program can be notified when the archives finish loading.

Prototype

ihArchiveRegisterLoadCallback {

ihServerHandle hServer, // server handle returned from previous call to ihServerConnect 

ihArchiveLoadCallbackFunction CallbackFunction,

void *UserParameter
);

Remarks

You need to have a callback or a function with the same signature as ihArchiveLoadCallback function, and then pass it to ihArchiveRegisterLoadCallback to register that function as a callback.

Returns

Returns StatusMessage
ihSTATUS_OK If the option was successfully read.
ihSTATUS_ACCESS_DENIEDIf you are not allowed to perform the operations. For most options you need to be a member of the ihArchiveAdmins group
ihSTATUS_API_TIMEOUTIf the option could not be read. You can try again later.
ihSTATUS_NOT_CONNECTED If you are not currently connected to the Data Archiver.
ihSTATUS_FAILEDFor any other type of error.