Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Importing Enumerated Sets
About this task
The Import Enumerated Sets function enables you to create or modify enumerated sets in the Historian Server. You can also add and modify sets using the Historian Administrator. See Working with Enumerated Sets.
Procedure
Select Administration and then select Import Enumerated Sets... from the Historian menu.
A message box appears asking you to confirm whether to import the sets.
Click Yes to initiate the operation.
If successful, a dialog box appears with the message, Import Enumerated Sets Succeeded confirming completion of the import function.
Click OK to close the dialog box. If errors on the import occur, a dialog box appears detailing the issues encountered during the import.