Relative Time Entries
When entering the Start and End times for Excel Add-in queries and exports, you can already enter them as exact literal dates and times such as “1/28/14 09:00:00
” in the query dialogs like Query Calculated Data, or you can use a cell reference to an exact time, or use an Excel function such as =Now()
or =Today()
. Apart from the mentioned ways, you can use relative time entries using a base value and an offset value as described in the following tables.
For example, you can use Yesterday+8H
for 8am yesterday or Now-15m
for 15 minutes before the current time. The typical use of a relative time entry, is to type the time values using a base and an offset into the start and end time of the Query dialogs or Export dialog, instead of having to put =Now()
or =Today()
in a cell and making a cell reference to that, or use the base Monday
to produce weekly reports.
Base Values
Base Value | Description |
---|---|
Now | The current date and time. |
Today | The current date at midnight. |
Yesterday | The previous day at midnight. |
Sunday | Today or the most recent Sunday at midnight. |
Monday | Today or the most recent Monday at midnight. |
Tuesday | Today or the most recent Tuesday at midnight. |
Wednesday | Today or the most recent Wednesday at midnight. |
Thursday | Today or the most recent Thursday at midnight. |
Friday | Today or the most recent Friday at midnight. |
Saturday | Today or the most recent Saturday at midnight. |
Offset Values
Offset Value | Description |
---|---|
d |
One 24 hour day |
h |
One hour |
m |
One minute |
s |
One second |