Differences Between the Web Admin and Historian Administrator
The Historian Web Admin Console provides a web-based user interface to Historian that permits you to monitor, supervise, archive, retrieve, and control data gather functions from the server, a client, or one or more remote web-based nodes.
There are some differences between the Historian Web Admin Console and the Windows-based Historian Administrator.
Note: All actions are common regardless of interface used, and any configuration done in one Administrator shows up in the other when the functionality is shared.
Available Only in the Web Admin Console | Available only in the Windows Historian Administrator |
---|---|
Diagnostic Dashboard | Single Interface to many servers |
Ability to Add/Configure Mirror | Calculation Tab under Tags, with the ability to create a calculated tag |
- | Tag Security Administration, with the ability to assign read/write/administer groups to a tag or set of tags |
- | Ability to define enumerated sets |
- | Ability to define user-defined types |
- | Ability to configure your HDA server |