Set Alarm Property Function
The Set Alarm Property
function will set the value of the selected alarm property. It will take the inputs shown in the following table.
Input | Description |
---|---|
Property | Specifies a property to get from the alarm object. If VendorAttribute is selected, additional list boxes will appear. |
Value | Specifies the property's new value. |
Attribute | Specifies the vendor attribute to set. This list box will appear if you have selected VendorAttribute in the Property list box. |
Value Type | Specifies the data type for the vendor attribute. Valid data types are:
|
Note: The
Set Alarm Property
function will not automatically save changes to the alarm object. To save changes to the alarm object, you must use the Update Alarm function.