Next Alarm Function
The Next Alarm
function will return the next alarm for a tag on or after a given time stamp. It will take the inputs shown in the following table.
Input | Description |
---|---|
Input Type | Specifies whether to manually input properties, or draw them from an existing alarm object. If Use Alarm Object Data is selected, the Source/Tag Name, Condition, and Relative Time fields will be disabled. |
Query By | Specifies whether to query by the alarm source or tag name. |
Source/ Tag Name | Specifies the source or tag name to query by. This field will change depending on what is selected in the Query By list box. |
Data Source | Specifies the data source to query by. This field will appear if Data Source is selected in the Query By list box. |
Condition | Specifies a condition to query by. |
Relative Time | Specifies a relative time to query by. |