Data Types

The following table lists the data types recommended for use with Historian.

OPC HDA Collector Data TypeRecommended Data Type in Historian
I1- 16 bit signed integer Single Integer
I4- 32 bit signed integer Double Integer
R8- 64 bit double floatSingle Float
UI2- 16 bit unsigned single integer Double Float
UI4- 32 bit unsigned double integer Unsigned Integer
UI8- 64 bit unsigned quad integerUnsigned Double Integer
I8- 64 bit quad integerQuad Integer
BSTRVariable Sting
BOOLBoolean
I1- 8 bit single integerByte
Note: The OPC HDA Collector requests data from the OPC HDA server in the native data type. The OPC HDA collector then converts the received value to a Historian Data Type before sending it to the data archiver.